LX2160A boot loader location

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LX2160A boot loader location

Jump to solution
3,019 Views
dmitri_lechtchinski
Contributor III

Hello,

Which devices can be used for loading boot loader image from on SoC startup? (XSPI, ...?)

Can an image be loaded from NVMe device?

Thanks,
Dmitri

0 Kudos
Reply
1 Solution
3,013 Views
ufedor
NXP Employee
NXP Employee

Please refer to the QorIQ LX2160A Reference Manual, Table 13. RCW Source and Flash Mode Encodings.

> Can an image be loaded from NVMe device?

No.

View solution in original post

1 Reply
3,014 Views
ufedor
NXP Employee
NXP Employee

Please refer to the QorIQ LX2160A Reference Manual, Table 13. RCW Source and Flash Mode Encodings.

> Can an image be loaded from NVMe device?

No.