LX2160A System Memory Map

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LX2160A System Memory Map

Jump to solution
3,766 Views
156614400
Contributor III

in  LX2160ARM.pdf ,  System Memory Map,   the ddr ram map the 0x0000_8000_0000  ,  but this region  is only 2G.    LX2160A-RDB board have 2 ddr slot,  if have 256G  ddr ,   what address it map ???

the ddr ram  is  maped to diffrent  divided  address ??

like this ?

0x0000_8000_0000 ------   0x0000_9FFF_FFFF      (2G)
0x0020_8000_0000 ------   0x003F_FFFF_FFFF      (128G)

0x0060_0000_0000 ----               (126G)

thanks

Tags (1)
0 Kudos
Reply
1 Solution
3,712 Views
ufedor
NXP Employee
NXP Employee

> the ddr ram  is  maped to diffrent  divided  address ??

Yes - refer to the QorIQ LX2160A Reference Manual, 2.2 System Memory Map.

According to the ARM Architecture SoC address to DRAM address remapping is preformed for the LX2160A as follows:

SoC Address

Size

Address presented to the DDR Controller

0x00_8000_0000 - 0x00_FFFF_FFFF

2GB

0x00_0000_0000 - 0x00_7FFF_FFFF

0x20_8000_0000 - 0x3F_FFFF_FFFF

126GB

0x00_8000_0000 - 0x1F_FFFF_FFFF

0x60_0000_0000 - 0x7F_FFFF_FFFF

128GB

0x20_0000_0000 - 0x3F_FFFF_FFFF

View solution in original post

1 Reply
3,713 Views
ufedor
NXP Employee
NXP Employee

> the ddr ram  is  maped to diffrent  divided  address ??

Yes - refer to the QorIQ LX2160A Reference Manual, 2.2 System Memory Map.

According to the ARM Architecture SoC address to DRAM address remapping is preformed for the LX2160A as follows:

SoC Address

Size

Address presented to the DDR Controller

0x00_8000_0000 - 0x00_FFFF_FFFF

2GB

0x00_0000_0000 - 0x00_7FFF_FFFF

0x20_8000_0000 - 0x3F_FFFF_FFFF

126GB

0x00_8000_0000 - 0x1F_FFFF_FFFF

0x60_0000_0000 - 0x7F_FFFF_FFFF

128GB

0x20_0000_0000 - 0x3F_FFFF_FFFF