LX2160A Serdes Clock type

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LX2160A Serdes Clock type

1,778件の閲覧回数
jack_huang1
Contributor IV

Hello,

        Please confirm whether the reference clock interface of Serdes is LVDS interface or LVPECL interface, thank you!

0 件の賞賛
返信
1 返信

1,771件の閲覧回数
r8070z
NXP Employee
NXP Employee

The differential SerDes reference clock inputs are DC-coupled, High-Speed Current Steering Logic (HCSL) compatible. In addition to the HCSL-type clock driver chip, many other low-voltage, differential output driver type clock chips, from various manufacturers, can be used (including LVDS and LVPECL). Please see the nxp app.note AN4311 SerDes Reference Clock Interfacing and HSSI Measurements Recommendations.

0 件の賞賛
返信