LS1043ARDB: P4 PCIe-x1 extension cable

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043ARDB: P4 PCIe-x1 extension cable

915 Views
ts1234
Contributor III
I am trying to use a PCIe-x1 device on P4 of the LS1043ARDB, with the help of a PCIe-x1 extension cable, but I am getting the continuous stream of the following kernel errors. 
How do I fix this? (Device works without the extension cable. This cable works on PC)
 
[  161.320269] pcieport 0001:00:00.0: AER:   device [1957:8080] error status/mask=00000001/00006000
[  161.329059] pcieport 0001:00:00.0: AER:    [ 0] RxErr
[  161.335592] pcieport 0001:00:00.0: AER: Multiple Corrected error received: 0001:00:00.0
[  161.343604] pcieport 0001:00:00.0: AER: PCIe Bus Error: severity=Corrected, type=Physical Layer, (Receiver ID)
[  161.353607] pcieport 0001:00:00.0: AER:   device [1957:8080] error status/mask=00000001/00006000
[  161.362399] pcieport 0001:00:00.0: AER:    [ 0] RxErr
[  161.368930] pcieport 0001:00:00.0: AER: Multiple Corrected error received: 0001:00:00.0
[  161.376944] pcieport 0001:00:00.0: AER: PCIe Bus Error: severity=Corrected, type=Physical Layer, (Receiver ID)
 
0 Kudos
Reply
0 Replies