LX2160A Serdes Clock type

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LX2160A Serdes Clock type

1,779 Views
jack_huang1
Contributor IV

Hello,

        Please confirm whether the reference clock interface of Serdes is LVDS interface or LVPECL interface, thank you!

0 Kudos
Reply
1 Reply

1,772 Views
r8070z
NXP Employee
NXP Employee

The differential SerDes reference clock inputs are DC-coupled, High-Speed Current Steering Logic (HCSL) compatible. In addition to the HCSL-type clock driver chip, many other low-voltage, differential output driver type clock chips, from various manufacturers, can be used (including LVDS and LVPECL). Please see the nxp app.note AN4311 SerDes Reference Clock Interfacing and HSSI Measurements Recommendations.

0 Kudos
Reply