LSDK v2.0: Linux Ethernet Independent Mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LSDK v2.0: Linux Ethernet Independent Mode

3,404 次查看
ckloecker
Contributor II

We use LSDK v2.0 17.03 and 20.04 on an LS1046A based platform. We would like to enable Ethernet "Independent Mode" (IM) which is supported according to LSDKUG_Rev20.04_290520. There is also some source code pointing to IM support in the Linux kernel, e.g. drivers/net/ethernet/freescale/sdk_fman/Peripherals/FM/Port/fm_port_im.c.

However, we do not see any way to enable this mode (e.g. via device tree). We also have no idea how to obtain the source code for the mentioned "dpaa_eth_im.ko" kernel module.

How can we enable the Ethernet Independent Mode in Linux and/or where can the "dpaa_eth_im.ko" source code be found?

标签 (1)
标记 (3)
5 回复数

3,374 次查看
ckloecker
Contributor II

Thank you very much!

Is it also compatible to LSDK 17.03?

0 项奖励
回复

3,372 次查看
yipingwang
NXP TechSupport
NXP TechSupport

It is not compatible with SDK 2.0 1703.

0 项奖励
回复

3,369 次查看
ckloecker
Contributor II

Is Independent Mode supported in LSDK v2.0 1703? If so, how can it be enabled?

0 项奖励
回复

3,379 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the step by step user manual in section "8.2.5.2.8.2.3.3 Independent-Mode" in LSDKUG_Rev20.04.pdf.

Please refer to the attachment for "dpaa_eth_im.ko" source code.

0 项奖励
回复

3,343 次查看
ckloecker
Contributor II

The source code is not compatible to Linux kernel 5.4.3 used in LSDK 20.04. I needed the following changes for compilation:

--- a/dpaa_eth_im.c
+++ b/dpaa_eth_im.c
@@ -753,6 +753,7 @@ static int init_phy(struct net_device *dev)
 {
     struct fm_im_private* priv = netdev_priv(dev);
     u32 supported;
+    u32 tmp_mask_legacy;
 
     priv->oldlink = 0;
     priv->oldspeed = 0;
@@ -774,8 +775,14 @@ static int init_phy(struct net_device *dev)
     }
 
     /* Remove any features not supported by the controller */
-    priv->phydev->supported &= supported;
-    priv->phydev->advertising = priv->phydev->supported;
+    ethtool_convert_link_mode_to_legacy_u32(&tmp_mask_legacy,
+                                            priv->phydev->supported);
+    tmp_mask_legacy &= supported;
+    ethtool_convert_legacy_u32_to_link_mode(priv->phydev->supported,
+                                            tmp_mask_legacy);
+
+    ethtool_convert_legacy_u32_to_link_mode(priv->phydev->advertising,
+                                            supported);
 
     return 0;
 }

Haven't tested it yet.

Are you sure that the module is compatible with LSDK 20.04? Git metadata suggests that it was written for LSDK 19.06.

0 项奖励
回复