LS2088A Reference Design Board Memory Size Limitation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS2088A Reference Design Board Memory Size Limitation

ソリューションへジャンプ
1,613件の閲覧回数
jason_zhao
Contributor I

Hello everyone,

We are planning to buy several LS2088A reference design boards for our development. Then I noticed that the spec of the board says the memory size is 8GB.

https://www.nxp.com/design/qoriq-developer-resources/layerscape-ls2088a-reference-design-board:LS208...

But the spec of the processor does not mention memory size limit.

https://www.nxp.com/docs/en/data-sheet/LS2088A.pdf

Since our applications might need more than 8GB memory. We are trying to see if the memory size limit is due to the broad or the processor. If due to the board if there any way to us to get a board with the same processor but with 16GB+ memory?

Thank you.

Jason   

 

0 件の賞賛
返信
1 解決策
1,609件の閲覧回数
ufedor
NXP Employee
NXP Employee

Picture in the Specifications section shows sizes of DIMM modules.

The picture is out-of-date - currently LS2088ARDB-PC is equipped with three 16GB DIMM modules which gives 32GB of main memory (third DIMM is intended for use by DPAA2).

For maximum supported memory sizes please refer to the QorIQ LS2088A Reference Manual, 12.6.1.1 Supported DDR SDRAM Organizations.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,610件の閲覧回数
ufedor
NXP Employee
NXP Employee

Picture in the Specifications section shows sizes of DIMM modules.

The picture is out-of-date - currently LS2088ARDB-PC is equipped with three 16GB DIMM modules which gives 32GB of main memory (third DIMM is intended for use by DPAA2).

For maximum supported memory sizes please refer to the QorIQ LS2088A Reference Manual, 12.6.1.1 Supported DDR SDRAM Organizations.

0 件の賞賛
返信