LS2088A - QUERY ON RTC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS2088A - QUERY ON RTC

1,693件の閲覧回数
preethi_rajagop
Contributor I

Hi,

I am working in LS2088A based project. I have doubt in RTC. There exist a pin TA_BB_RTC  - pin K19. In datasheet, it is referred as reverved and given a note to connect it ground. But, Is this anything regarding the optional RTC clock? Should we give the provision of optional Oscillator?

If not, why is the name TA_BB_RTC. Please clarify.

ラベル(1)
0 件の賞賛
返信
1 返信

1,589件の閲覧回数
ufedor
NXP Employee
NXP Employee

TA_BB_RTC has been de-featured. Since there were customers that have already designed with the pin name, it was decided to keep the pin name.
Note 15 is correct. New designs should disregard the reference board on this and be implemented in accordance with the processor's Data Sheet.

0 件の賞賛
返信