LS2080A capability

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,654件の閲覧回数
JHY
Contributor IV

Hello, experts.

LS2080A has total 16 serdes lanes for variable purpose.

So, please confirm below options are able to be implemented in LS2080A.

1. simultaneously up to 5.8G input to LS2080A and up to 2.4G output from LS2080A by PCIE.

2. vice versa 5.8G output from LS2080A and up to 2.4G input to LS2080A by PCIE

Best regards.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
3,424件の閲覧回数
bpe
NXP Employee
NXP Employee

LS2080 can support much higher than you specified data rates at the SecDes and on-chip interconnect

levels. I's ability to support a certain type of protocol or application  at some  data rate, however,  depends on

both the application/protocol type and the implementation. Contact a distributor in your region for

advanced performance information.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,425件の閲覧回数
bpe
NXP Employee
NXP Employee

LS2080 can support much higher than you specified data rates at the SecDes and on-chip interconnect

levels. I's ability to support a certain type of protocol or application  at some  data rate, however,  depends on

both the application/protocol type and the implementation. Contact a distributor in your region for

advanced performance information.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,424件の閲覧回数
JHY
Contributor IV

One more question.

It has 4 PCIE controller.

Is it possible to use 2 lanes PCIE x 4 at single serdes block like below?

2x4.jpg

0 件の賞賛
返信
3,424件の閲覧回数
bpe
NXP Employee
NXP Employee

This is too confused. Two lanes mean PCIe x2. PCIe x4 requires four lanes. The picture displays four PCIe controllers connected

to an 8-lane SerDes, which obviously can be done in several bus width combinations. Refer to the chip Manual, Section 25.1.2.1 for available SerDes protocol combinations.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------