LS1088 Throughput test setup

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1088 Throughput test setup

2,146 Views
stadium_aquino
Contributor IV

In the DPAA2 Low-level hardware reference manual section 7.3.1, the LS1088A is specified as supporting 30Mpps through its two 10G ports with 64B packets. What is the test setup necessary to achieve this? I am unable to achieve more than around 2Mpps. Does the DPAA2 need to be configured in a specific way? Are there patches which must be applied to Linux? Are you using the kernel networking stack or DPDK?

Labels (1)
0 Kudos
Reply
1 Reply

2,123 Views
andrei_skok
NXP Employee
NXP Employee

The numbers specified in the DPAA2 Low-level hardware reference manual are the maximum values for the  WRIOP engine version present in  LS1088.

0 Kudos
Reply