LS1088 Throughput test setup

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1088 Throughput test setup

2,134件の閲覧回数
stadium_aquino
Contributor IV

In the DPAA2 Low-level hardware reference manual section 7.3.1, the LS1088A is specified as supporting 30Mpps through its two 10G ports with 64B packets. What is the test setup necessary to achieve this? I am unable to achieve more than around 2Mpps. Does the DPAA2 need to be configured in a specific way? Are there patches which must be applied to Linux? Are you using the kernel networking stack or DPDK?

ラベル(1)
0 件の賞賛
返信
1 返信

2,111件の閲覧回数
andrei_skok
NXP Employee
NXP Employee

The numbers specified in the DPAA2 Low-level hardware reference manual are the maximum values for the  WRIOP engine version present in  LS1088.

0 件の賞賛
返信