LS1046ardb USB function

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1046ardb USB function

2,479 次查看
abanwer
Contributor I

Hi,

   I am working on USB function driver for ls1046ardb board, the issue I am facing is that I don't receive a disconnect interrupt when cable is unplugged from host. I have enable the disconnect interrupt from DEVTEN register. I am using USB1 device. Are there any other settings that need to be done for enabling the disconnect interrupt. Connect and reset interrupts are working fine. 

标签 (1)
0 项奖励
回复
2 回复数

2,197 次查看
Pavel
NXP Employee
NXP Employee

Look at the Section 33.4.3.1.1 of the LS1046a Reference Manual. Do you use similar command sequence for USB 3.0 device initialization?

Look at attached file. It is LS1043a USB driver code from NXP SDK 2.0 Linux BSP. Similar code can be used on the LS1046a board.

See gatged.c file.

 


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,197 次查看
abanwer
Contributor I

Thanks I will look into it.

0 项奖励
回复