LS1046A QSPI signal state when PORESET_B asserted

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1046A QSPI signal state when PORESET_B asserted

1,845 次查看
sabine_s
Contributor III

For the LS1046A, when PORESET_B is asserted, are all QSPI signals in high impedance state?

I am wondering if I can program QSPI RCW/PBI/boot flash using an external master if I apply power and keep PORESET_B asserted. Any problems doing it this way?

标签 (1)
1 回复

1,690 次查看
ufedor
NXP Employee
NXP Employee

Yes, external master can program SPI Flash connected to QSPI when PORESET_B is asserted.