LS1046A custom board converting cwflash init to PBI commands

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046A custom board converting cwflash init to PBI commands

ソリューションへジャンプ
1,798件の閲覧回数
JRRandall
Contributor III

Greetings.

we are trying to bring up our custom board based off the LS1046A.  We have had success using cwflash.py and custom scripts based on the LS1046A FRWY init.  The question we have is if there is any automatic or easy way to convert the large number of CCSR address space commands in the DDR4 init script that cwflash uses into PBI commands for running in the BL2/PBL on our target board?

ラベル(2)
0 件の賞賛
返信
1 解決策
1,778件の閲覧回数
ufedor
NXP Employee
NXP Employee

There is no automatic way to perform required conversion.

元の投稿で解決策を見る

1 返信
1,779件の閲覧回数
ufedor
NXP Employee
NXP Employee

There is no automatic way to perform required conversion.