LS1046A custom board converting cwflash init to PBI commands

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046A custom board converting cwflash init to PBI commands

Jump to solution
1,789 Views
JRRandall
Contributor III

Greetings.

we are trying to bring up our custom board based off the LS1046A.  We have had success using cwflash.py and custom scripts based on the LS1046A FRWY init.  The question we have is if there is any automatic or easy way to convert the large number of CCSR address space commands in the DDR4 init script that cwflash uses into PBI commands for running in the BL2/PBL on our target board?

Labels (2)
0 Kudos
Reply
1 Solution
1,769 Views
ufedor
NXP Employee
NXP Employee

There is no automatic way to perform required conversion.

View solution in original post

1 Reply
1,770 Views
ufedor
NXP Employee
NXP Employee

There is no automatic way to perform required conversion.