LS1046A boundary scan register TDR layout

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1046A boundary scan register TDR layout

跳至解决方案
1,354 次查看
larsthestrup
Contributor III

I need to set the TDR register via the IOCONFIG command, but can not find the register layout.
I have read the AN5352 application note, but it is for another CPU with register length of 105, LS1046A has a register length of 162.
BR Lars Thestrup

0 项奖励
回复
1 解答
1,349 次查看
ufedor
NXP Employee
NXP Employee
0 项奖励
回复
1 回复
1,350 次查看
ufedor
NXP Employee
NXP Employee
0 项奖励
回复