LS1046A boundary scan register TDR layout

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046A boundary scan register TDR layout

Jump to solution
2,024 Views
larsthestrup
Contributor III

I need to set the TDR register via the IOCONFIG command, but can not find the register layout.
I have read the AN5352 application note, but it is for another CPU with register length of 105, LS1046A has a register length of 162.
BR Lars Thestrup

0 Kudos
Reply
1 Solution
2,019 Views
ufedor
NXP Employee
NXP Employee
0 Kudos
Reply
1 Reply
2,020 Views
ufedor
NXP Employee
NXP Employee
0 Kudos
Reply