LS1046A-RDB svd file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1046A-RDB svd file

1,890 次查看
ameerhamza
Contributor III

I need svd file for ls1046a-rdb which i have to port to custom sprite for register view, but i could not find anywhere on internet. For reference: SVD file for LPC is available at: cmsis-svd/data/NXP at master · posborne/cmsis-svd · GitHub. Any help would be highly appreciated.

Best Regards,

Hamza.

标签 (1)
0 项奖励
回复
1 回复

1,763 次查看
Pavel
NXP Employee
NXP Employee

NXP SDK for the LS1046a and CodeWarrior for QorIQ ARM do no not use SVD files. There are no SVD file for the LS1046a.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复