LS1046A-RDB svd file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046A-RDB svd file

1,865件の閲覧回数
ameerhamza
Contributor III

I need svd file for ls1046a-rdb which i have to port to custom sprite for register view, but i could not find anywhere on internet. For reference: SVD file for LPC is available at: cmsis-svd/data/NXP at master · posborne/cmsis-svd · GitHub. Any help would be highly appreciated.

Best Regards,

Hamza.

ラベル(1)
0 件の賞賛
返信
1 返信

1,738件の閲覧回数
Pavel
NXP Employee
NXP Employee

NXP SDK for the LS1046a and CodeWarrior for QorIQ ARM do no not use SVD files. There are no SVD file for the LS1046a.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信