LS1046A-RDB svd file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046A-RDB svd file

1,923 Views
ameerhamza
Contributor III

I need svd file for ls1046a-rdb which i have to port to custom sprite for register view, but i could not find anywhere on internet. For reference: SVD file for LPC is available at: cmsis-svd/data/NXP at master · posborne/cmsis-svd · GitHub. Any help would be highly appreciated.

Best Regards,

Hamza.

Labels (1)
0 Kudos
Reply
1 Reply

1,796 Views
Pavel
NXP Employee
NXP Employee

NXP SDK for the LS1046a and CodeWarrior for QorIQ ARM do no not use SVD files. There are no SVD file for the LS1046a.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply