LS1046A QDMA Max Performance

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046A QDMA Max Performance

ソリューションへジャンプ
2,309件の閲覧回数
JSKIM
Contributor III

I just wonder about qdma max performance.

I have tested QDMA on LS1046A with dma one channel. and the result is 3522240 KByte/s.

Is this result QDMA near maximum performance?

0 件の賞賛
返信
1 解決策
2,292件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the following QDMA performance test data.

Memory 64B (KB) 512B (KB) 1KB 2KB 4KB 16KB 64KB 1M
DDR->DDR 774.8 Mbps 5279.6 Mbps 8671.1 Mbps 15112.7 Mbps 28929.2 Mbps 30340.5 Mbps 26293.4 Mbps 21256 Mbps

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,873件の閲覧回数
BarryD
Contributor I

Can you provide more details on how you measured this max qdma performance, such as which kernel, which driver, what app was run to make the measurement?

0 件の賞賛
返信
2,293件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the following QDMA performance test data.

Memory 64B (KB) 512B (KB) 1KB 2KB 4KB 16KB 64KB 1M
DDR->DDR 774.8 Mbps 5279.6 Mbps 8671.1 Mbps 15112.7 Mbps 28929.2 Mbps 30340.5 Mbps 26293.4 Mbps 21256 Mbps
0 件の賞賛
返信