LS1046A QDMA Max Performance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046A QDMA Max Performance

Jump to solution
2,359 Views
JSKIM
Contributor III

I just wonder about qdma max performance.

I have tested QDMA on LS1046A with dma one channel. and the result is 3522240 KByte/s.

Is this result QDMA near maximum performance?

0 Kudos
Reply
1 Solution
2,342 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the following QDMA performance test data.

Memory 64B (KB) 512B (KB) 1KB 2KB 4KB 16KB 64KB 1M
DDR->DDR 774.8 Mbps 5279.6 Mbps 8671.1 Mbps 15112.7 Mbps 28929.2 Mbps 30340.5 Mbps 26293.4 Mbps 21256 Mbps

View solution in original post

0 Kudos
Reply
2 Replies
1,923 Views
BarryD
Contributor I

Can you provide more details on how you measured this max qdma performance, such as which kernel, which driver, what app was run to make the measurement?

0 Kudos
Reply
2,343 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the following QDMA performance test data.

Memory 64B (KB) 512B (KB) 1KB 2KB 4KB 16KB 64KB 1M
DDR->DDR 774.8 Mbps 5279.6 Mbps 8671.1 Mbps 15112.7 Mbps 28929.2 Mbps 30340.5 Mbps 26293.4 Mbps 21256 Mbps
0 Kudos
Reply