LS1046A PCIe PEX Internal registers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046A PCIe PEX Internal registers

2,711件の閲覧回数
keithw
Contributor III

Is there any documentation for the PEX module internal configuration space registers outside of the LS1046A Reference Manual?  The RTOS that I am using (VxWorks) is writing to a couple of registers that I cannot find documentation for -- PCIE_PL_PLCR (0x710) and PCIE_PL_G2CR (0x80C). 

I am having trouble getting the PCIe link established on our custom board and the link appears to be breaking down after a write to the PCIE_PL_G2CR.

0 件の賞賛
返信
4 返答(返信)

2,632件の閲覧回数
keithw
Contributor III

I have not attempted with the Linux BSP, but the fact remains that there appear to be undocumented registers that affect the behavior of the system.  I am really looking for documentation for these registers. I have managed to establish a single-lane PCIe link between our LS1046A and FPGA although I have not been successful yet on getting all four lanes working (but that is unrelated to this issue).

0 件の賞賛
返信

2,582件の閲覧回数
Oswalag
NXP TechSupport
NXP TechSupport

Sorry, we do not have resources to support third-party software.
Please address your question to the Wind River technical support, they should be able to provide the description of the mentioned registers, from our side the processor's RM is the only source.

0 件の賞賛
返信

2,578件の閲覧回数
keithw
Contributor III

Ok, in case anyone runs across this problem in the future, these registers are documented in other NXP processor registers.  The i.MX7 manual contains definitions for these registers.  It appears the same IP core is used between these two.

I'm not sure why the NXP LS1046A reference manual doesn't document all of the registers that are present.

0 件の賞賛
返信

2,639件の閲覧回数
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

Is the issue present If you try with our Linux BSP ?

0 件の賞賛
返信