LS1046A & LS1046A-RDB Available Memory

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1046A & LS1046A-RDB Available Memory

跳至解决方案
2,166 次查看
ahanson
Contributor I

I'm currently working with the LS1046A-RDB reference board design kit provided by eInfoChips.   The application notes on the system defines that the available memory for the single physical bank is 8-GB.  For the reference kit, is this the maximum available memory or can I swap the memory module with a larger DDR4?  

When designing my own board off the LS1046A QorIQ Layerscape, what's the maximum physical bank count and memory capacity per bank that I can put into my design?

0 项奖励
回复
1 解答
2,016 次查看
ufedor
NXP Employee
NXP Employee

Maximum supported LS1046A DDR controller 64-bit bank size is 16 GB.

The DDR controller supports 4 banks.

Refer to the QorIQ LS1046A Reference Manual, Table 15-9. Supported SDRAM Device Configurations, DDR4.

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,017 次查看
ufedor
NXP Employee
NXP Employee

Maximum supported LS1046A DDR controller 64-bit bank size is 16 GB.

The DDR controller supports 4 banks.

Refer to the QorIQ LS1046A Reference Manual, Table 15-9. Supported SDRAM Device Configurations, DDR4.

0 项奖励
回复