LS1046A & LS1046A-RDB Available Memory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046A & LS1046A-RDB Available Memory

ソリューションへジャンプ
2,176件の閲覧回数
ahanson
Contributor I

I'm currently working with the LS1046A-RDB reference board design kit provided by eInfoChips.   The application notes on the system defines that the available memory for the single physical bank is 8-GB.  For the reference kit, is this the maximum available memory or can I swap the memory module with a larger DDR4?  

When designing my own board off the LS1046A QorIQ Layerscape, what's the maximum physical bank count and memory capacity per bank that I can put into my design?

0 件の賞賛
返信
1 解決策
2,026件の閲覧回数
ufedor
NXP Employee
NXP Employee

Maximum supported LS1046A DDR controller 64-bit bank size is 16 GB.

The DDR controller supports 4 banks.

Refer to the QorIQ LS1046A Reference Manual, Table 15-9. Supported SDRAM Device Configurations, DDR4.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,027件の閲覧回数
ufedor
NXP Employee
NXP Employee

Maximum supported LS1046A DDR controller 64-bit bank size is 16 GB.

The DDR controller supports 4 banks.

Refer to the QorIQ LS1046A Reference Manual, Table 15-9. Supported SDRAM Device Configurations, DDR4.

0 件の賞賛
返信