LS1046A 1000Base-KX Mode with Linux Mainline

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046A 1000Base-KX Mode with Linux Mainline

ソリューションへジャンプ
1,358件の閲覧回数
timsalabim
Contributor II

Hello, 

one of our customers want to use 1000Base-KX with the LS1046A CPU.  When researching I found the following comment in the 6.12.33 Linux Mainline kernel in    /tree/drivers/net/ethernet/freescale/fman/fman_memac.c

/* TODO: The following interface modes are supported by (some) hardware
	 * but not by this driver:
	 * - 1000BASE-KX
	 * - 10GBASE-KR
	 * - XAUI/HiGig
	 */


This comment is missing in the QoriQ Linux kernel repository so I'm wondering if it will be possible to use Linux Mainline kernel with 1000Base-KX. 

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,339件の閲覧回数
LFGP
NXP TechSupport
NXP TechSupport
Dear @timsalabim,
Unfortunately it is not possible to use it with that release, please use an older release, such the 6.1.55

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,340件の閲覧回数
LFGP
NXP TechSupport
NXP TechSupport
Dear @timsalabim,
Unfortunately it is not possible to use it with that release, please use an older release, such the 6.1.55
0 件の賞賛
返信