LS1046 Small packet transmission -- Network packet loss

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046 Small packet transmission -- Network packet loss

ソリューションへジャンプ
3,970件の閲覧回数
Hmc510
Contributor II

LS1046:

I tried using the iperf3 tool to test TCP packet transmission.

find some retransmission in speed 10Mb/s . packet size is 60 byte.(net link is 100Mbps)

Hmc510_0-1683529418171.png

and the ethtool notify no drop\error packets find:

Hmc510_1-1683529489188.png

I am trying to count the number of network connections between PCs and board 1046:(use cmd netstat -i)

iperf3 notify the "Retr=13"

PC: Tx = 15506

1046: Rx= 15493 . (obvious lost "13" )

and my net chip is YT8614 use Serdes 0x3040 channel B(QSGMII x4).It provides network frame counting,and I read the regs the Rx packet is 15506.

So the packet received by the network chip(YT8614) is correct. and ethtool notify Rx=15493(lost 13) ,and (drop+error = 0).

Has the data packet been lost elsewhere? Serdes\Bman\Kernel? Do they have packet counting function for debug.

 

Thanks

 

 

0 件の賞賛
返信
1 解決策
3,849件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
5 返答(返信)
3,939件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
3,936件の閲覧回数
Hmc510
Contributor II

Thank you for your reply

1. I have used this document and still have no leads.

2. What do these numerical values represent

Hmc510_0-1683627332543.png

 

0 件の賞賛
返信
3,885件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Could you please share the LSDK version and kernel version info?

0 件の賞賛
返信
3,880件の閲覧回数
Hmc510
Contributor II

pakcet is LSDK 2108

linux 5.10

Hmc510_0-1683886813392.png

 

Hmc510_1-1683886842565.png

 

 

0 件の賞賛
返信
3,850件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信