LS1046 Nandflash Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046 Nandflash Problem

873件の閲覧回数
jack_huang1
Contributor IV

Dear:

      Our product uses NXP LS1046A and SDK uses LSDK2108. We have a problem: we plan to put uboot into qspiflash, and kernel, dtb and rootfs into 512MB nandflash. Nandflash is divided into three areas, the size of which is 16M, 48M and 448M. dtb file, kernel image and rootfs are placed respectively.

       The current problems is whether the build/Linux/Linux/arm64 / LS/Image  Or build/Linux/Linux/arm64 / LS/called burn into the nand flash - 5.10.35 - dirty,   If bootm $load_addr $fdtaddr is used after the uboot reads to the memory, the following error occurs Wrong Image Format for bootm command: ERROR: can't get kernel image!

         Which Image should be used as the boot parameter of bootm? How should I handle this?Thanks!

Best Regards!

0 件の賞賛
返信
0 返答(返信)