LS1046 Nandflash Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046 Nandflash Problem

872 Views
jack_huang1
Contributor IV

Dear:

      Our product uses NXP LS1046A and SDK uses LSDK2108. We have a problem: we plan to put uboot into qspiflash, and kernel, dtb and rootfs into 512MB nandflash. Nandflash is divided into three areas, the size of which is 16M, 48M and 448M. dtb file, kernel image and rootfs are placed respectively.

       The current problems is whether the build/Linux/Linux/arm64 / LS/Image  Or build/Linux/Linux/arm64 / LS/called burn into the nand flash - 5.10.35 - dirty,   If bootm $load_addr $fdtaddr is used after the uboot reads to the memory, the following error occurs Wrong Image Format for bootm command: ERROR: can't get kernel image!

         Which Image should be used as the boot parameter of bootm? How should I handle this?Thanks!

Best Regards!

0 Kudos
Reply
0 Replies