LS1046 INTERFACE WITH DDR4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046 INTERFACE WITH DDR4

ソリューションへジャンプ
4,503件の閲覧回数
Ellu24
Contributor III

Can I interface ls1046 with MT53D1024M32D4DT-046 DDR4.Datasheet is attached below. If possible, 1) 1) how data lines should be connected 

2) can I connect this with ls1046 since it doesn't have ECC.

0 件の賞賛
返信
1 解決策
4,498件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

MT53D1024M32D4DT-046 is an LPDDR4/LPDDR4X SDRAM. LS1046A only supports DDR4 and does not support LPDDR4/4X.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,494件の閲覧回数
Ellu24
Contributor III

Can you please suggest a DDR4 for me to use?

0 件の賞賛
返信
4,495件の閲覧回数
Ellu24
Contributor III

Thank you for the reply. So I am not able to use it, right?

0 件の賞賛
返信
4,499件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

MT53D1024M32D4DT-046 is an LPDDR4/LPDDR4X SDRAM. LS1046A only supports DDR4 and does not support LPDDR4/4X.

0 件の賞賛
返信