LS1046 CW-TAP Logic Levels

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046 CW-TAP Logic Levels

3,260 Views
matthej
Contributor II

Hi,

 

I am using the CW TAP module along with the CWH-CTP-CTX10-YE on my LS1046 design.

For a newer design, I need to add in a buffer between the TAP and the LS1046 processor.

Can you please provide me the logic levels so that I can ensure it will meet the specification?

This interface is running at 1.8V.

Thanks!

 

0 Kudos
Reply
5 Replies

3,221 Views
Chavira
NXP TechSupport
NXP TechSupport

Hello matthej!

We only have this document with that information but it is not that specific because the CodeWarrior Tap automatically supports system voltage levels from 1.2v to 3.3v

CodeWarrior<sup>®</sup> Tap - Fact Sheet (nxp.com)

Best regards!

0 Kudos
Reply

3,243 Views
matthej
Contributor II

I do not see where the logic levels (electrical specifications) are in this document. Can you please reference the page?

 

Thanks

Jeff

 

0 Kudos
Reply

3,231 Views
Chavira
NXP TechSupport
NXP TechSupport

Hello matthej!

In the next link you can download the datasheet for the LS1046.

# Layerscape® 1046A | NXP Semiconductors

In the page 51 you can see the table 4 for recommended operating conditions and for more specific information about the logic levels on this chip you can consult the page 151 for GPIO DC electrical characteristics

Best regards!

0 Kudos
Reply

3,227 Views
matthej
Contributor II

I am not looking for the LS1046 electrical specs I am looking for the CW Tap electrical specs which are not found in the manual you provided.

 

Thanks

 

0 Kudos
Reply

3,246 Views
Chavira
NXP TechSupport
NXP TechSupport

In the following link you can find the "CodeWarrior TAP Probe User Guide" in which you can find specifications and steps to configure the TAP Probe and be able to perform and view device information.

0 Kudos
Reply