LS1023 Setting for Qspi and IFC Bus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1023 Setting for Qspi and IFC Bus

1,755件の閲覧回数
kk_1123
Contributor I

First, I set the BOOT setting of RCW to Quad SPI(QSPI_A).

After CPU boots, I'd like to use IFC Bus. But the following pins of CPU are multiplexed:  QSPI_A_CS0/IFC_A16  

    QSPI_A_CS1/IFC_A17

If this goes on, I can't use IFC_A16,A17. To enable IFC_A16,A17,how should I do?

(I think there are some internal registers for mode setting, but I couldn't find them.)

Thank you.

0 件の賞賛
返信
1 返信

1,549件の閲覧回数
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @kk_1123,

 

If QuadSPI is selected for cfg_rcw_src then the IFC_GRP_F_EXT field must be set to 001 which means IFC signals signal can't be configured.

 

Regards

Mrudang Shelat

0 件の賞賛
返信