LS1046 CW-TAP Logic Levels

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046 CW-TAP Logic Levels

3,351件の閲覧回数
matthej
Contributor II

Hi,

 

I am using the CW TAP module along with the CWH-CTP-CTX10-YE on my LS1046 design.

For a newer design, I need to add in a buffer between the TAP and the LS1046 processor.

Can you please provide me the logic levels so that I can ensure it will meet the specification?

This interface is running at 1.8V.

Thanks!

 

0 件の賞賛
返信
5 返答(返信)

3,312件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hello matthej!

We only have this document with that information but it is not that specific because the CodeWarrior Tap automatically supports system voltage levels from 1.2v to 3.3v

CodeWarrior<sup>®</sup> Tap - Fact Sheet (nxp.com)

Best regards!

0 件の賞賛
返信

3,334件の閲覧回数
matthej
Contributor II

I do not see where the logic levels (electrical specifications) are in this document. Can you please reference the page?

 

Thanks

Jeff

 

0 件の賞賛
返信

3,322件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hello matthej!

In the next link you can download the datasheet for the LS1046.

# Layerscape® 1046A | NXP Semiconductors

In the page 51 you can see the table 4 for recommended operating conditions and for more specific information about the logic levels on this chip you can consult the page 151 for GPIO DC electrical characteristics

Best regards!

0 件の賞賛
返信

3,318件の閲覧回数
matthej
Contributor II

I am not looking for the LS1046 electrical specs I am looking for the CW Tap electrical specs which are not found in the manual you provided.

 

Thanks

 

0 件の賞賛
返信

3,337件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

In the following link you can find the "CodeWarrior TAP Probe User Guide" in which you can find specifications and steps to configure the TAP Probe and be able to perform and view device information.

0 件の賞賛
返信