LS1043ARGW SD TFA boot problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043ARGW SD TFA boot problem

Jump to solution
21,731 Views
hakjunoh
Contributor III

I have LS1043ARGW custom boards and LS1043ARDB-PD boards. I am trying to boot from an sd card.

And I need OP-TEE, so I have to boot with TFA. However, there is a problem that the boot does not work. So I built it as tfa, not SECURE_tfa. Of course the ASK binary works fine.

1. u-boot (Needed for building atf)

I made u-boot patch file with reference to RGW u-boot. And patched to u-boot LSDK-20.04.

Then I set to ls1043argw_tfa_config and built.

2. atf

atf LSDK-20.04 was built using the following options:

PLAT=ls1043ardb

BOOT_MODE=sd

RCW=(ls1043ardb-sdboot-rcw.bin) <- attached file

BL33=u-boot.bin

FIPTOOL=tools/fiptool/fiptool

CREATE_PBL=/plat/nxp/tools/create_pbl

BYTE_SWAP=/plat/nxp/tools/byte_swap

DEBUG=1

3. write to sd card

bl2_sd.pbl and fip.bin generated by building atf were written to the sd card.

Write to SD

dd if=/dev/zero of=/dev/mmcblk0 bs=1M count=10

dd if=bl2_sd.pbl of=/dev/mmcblk0 bs=512 seek=8
dd if=fip.bin of=/dev/mmcblk0 bs=512 seek=2048

4. boot

When booting this sd card from RDB

RDB boot log

INFO: RCW BOOT SRC is SD/EMMC
INFO: RCW BOOT SRC is SD/EMMC
INFO: Card detected successfully
INFO: init done:
INFO: time base 30 ms
NOTICE: Fixed DDR on board
INFO: Time after parsing SPD 4 ms
INFO: Time before programming controller 8 ms

NOTICE: 2 GB DDR4, 32-bit, CL=11, ECC off
INFO: Time used by DDR driver 18 ms
NOTICE: BL2: v1.5(debug):LSDK-20.04
NOTICE: BL2: Built : 07:46:25, May 7 2020
INFO: CALL: bl2_arch_setup
INFO: CALL: bl2_plat_preload_setup
INFO: Configuring TZASC-380
INFO: CALL: bl2_load_images
INFO: BL2: Doing platform setup
INFO: BL2: Loading image id 3
INFO: sd-mmc read done.
INFO: sd-mmc read done.

U-Boot 2019.10 (May 07 2020 - 07:46:23 +0100)

SoC: LS1043AE Rev1.1 (0x87920011)
Clock Configuration:
CPU0(A53):1600 MHz CPU1(A53):1600 MHz CPU2(A53):1600 MHz
CPU3(A53):1600 MHz
Bus: 300 MHz DDR: 1600 MT/s FMAN: 600 MHz
Reset Configuration Word (RCW):
00000000: 06100010 0c000000 00000000 00000000
00000010: 14550002 80004002 60106000 c1002000
00000020: 00000000 00000000 00000000 01030940
00000030: 00000000 00003004 00000096 00000001
Model: LS1043A RGW Board
Board: LS1043ARGW, boot from SD
Invalid setting
SERDES Reference Clocks:
SD1_CLK1 = 156.25MHZ, SD1_CLK2 = 100.00MHZ
DRAM: 1.9 GiB (DDR4, 32-bit, CL=11, ECC off)
Using SERDES1 Protocol: 5205 (0x1455)
SEC0: RNG instantiated
Flash: 128 MiB
NAND: 512 MiB
MMC: FSL_SDHC: 0
Loading Environment from MMC... *** Warning - bad CRC, using default environment

EEPROM: NXID v1
In: serial
Out: serial
Err: serial
Net:
MMC read: dev # 0, block # 18432, count 128 ...
Fman1: Data at 00000000f7a38f60 is not a firmware
PCIe0: pcie@3400000 disabled
PCIe1: pcie@3500000 Root Complex: no link
PCIe2: pcie@3600000 Root Complex: no link
No ethernet found.
Hit any key to stop autoboot: 0

but when booting from RGW

RGW boot log

?NFO: RCW BOOT SRC is SD/EMMC
INFO: RCW BOOT SRC is SD/EMMC
INFO: Card detected successfully
INFO: init done:
INFO: time base 30 ms
NOTICE: Fixed DDR on board
INFO: Time after parsing SPD 5 ms
INFO: Time before programming controller 8 ms

NOTICE: 2 GB DDR4, 32-bit, CL=11, ECC off
INFO: Time used by DDR driver 18 ms
NOTICE: BL2: v1.5(debug):LSDK-20.04
NOTICE: BL2: Built : 08:27:14, Apr 22 2020
INFO: Configuring TZASC-380
INFO: BL2: Doing platform setup
INFO: BL2: Loading image id 3
INFO: sd-mmc read done.
WARNING: Firmware Image Package header check failed.
WARNING: Failed to obtain reference to image id=3 (-2)
ERROR: BL2: Failed to load image (-2)
Authentication failure

I have looked at the operation problems of eSDHC, but confirmed that it works in 1bit little-endian mode on the source.
As a result of several boot checks, the ATF confirmed that the FIP header value was read from 0x10_0000.
In the case of RDB, the FIP header read the value of 0x10_0000 correctly, but it was confirmed that RGW reads the value of 0x10_0008.

I have not yet figured out what is causing this issue.

Please help me.

best regards.

Labels (1)
1 Solution
21,078 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello hakjun oh,

In the TF-A boot flow, DDR initialization is not required in U-Boot. DDR initialization is a part of TF-A.

DDR init code can be added to <atf_dir>/plat/nxp/soc-<soc-name>/<soc-name>ardb/ddr_init.c.

You need to modify ddr_raw_timing in atf/plat/nxp/soc-ls1043/ls1043ardb/ddr_init.c according to your custom board.

Thanks,

Yiping

 

 

View solution in original post

18 Replies
21,079 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello hakjun oh,

In the TF-A boot flow, DDR initialization is not required in U-Boot. DDR initialization is a part of TF-A.

DDR init code can be added to <atf_dir>/plat/nxp/soc-<soc-name>/<soc-name>ardb/ddr_init.c.

You need to modify ddr_raw_timing in atf/plat/nxp/soc-ls1043/ls1043ardb/ddr_init.c according to your custom board.

Thanks,

Yiping

 

 

21,078 Views
hakjunoh
Contributor III

Hi Yiping.

So, is the RAM timing problem the reason why BL2 Image is read from 0x10_0008 when LS1043ARGW is booted?

Thanks,

hakjun oh

0 Kudos
Reply
21,078 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello hakjun oh,

Yes, DDR initialization problem is the cause.

Thanks,

Yiping

0 Kudos
Reply
21,069 Views
hakjunoh
Contributor III

Yiping.

Unfortunately, the ram timing value has been changed, but the same message is output.

The source uses the MT40A512M8HX-093E, but our custom board uses the MT40A512M8RH-083E.

The changes are as follows.

plat/nxp/soc-ls1043/ls1043ardb/ddr_init.c

diff --git a/plat/nxp/soc-ls1043/ls1043ardb/ddr_init.c b/plat/nxp/soc-ls1043/ls1043ardb/ddr_init.c
index 705adb014..776204d57 100644
--- a/plat/nxp/soc-ls1043/ls1043ardb/ddr_init.c
+++ b/plat/nxp/soc-ls1043/ls1043ardb/ddr_init.c
@@ -92,33 +92,33 @@ int ddr_board_options(struct ddr_info *priv)
      return 0;
}

-/* DDR model number: MT40A512M8HX-093E */
+/* DDR model number: MT40A512M8RH-083E */
struct dimm_params ddr_raw_timing = {
      .n_ranks = 1,
      .rank_density = 2147483648u,
      .capacity = 2147483648u,
      .primary_sdram_width = 32,
-     .n_row_addr = 15,
-     .n_col_addr = 10,
+    .n_row_addr = 15, //row addressing
+    .n_col_addr = 10, //col addressing
      .bank_group_bits = 2,
      .burst_lengths_bitmask = 0x0c,
-     .tckmin_x_ps = 938,
-     .tckmax_ps = 1500,
+    .tckmin_x_ps = 834, //tck min
+    .tckmax_ps = 938, //tck max
      .caslat_x = 0x000DFA00,
-     .taa_ps = 13500,
-     .trcd_ps = 13500,
-     .trp_ps = 13500,
-     .tras_ps = 33000,
-     .trc_ps = 46500,
-     .twr_ps = 15000,
-     .trfc1_ps = 260000,
-     .trfc2_ps = 160000,
-     .trfc4_ps = 110000,
-     .tfaw_ps = 21000,
-     .trrds_ps = 3700,
-     .trrdl_ps = 5300,
-     .tccdl_ps = 5355,
-     .refresh_rate_ps = 7800000,
+    .taa_ps = 13320, //taa
+    .trcd_ps = 13320, //trcd
+    .trp_ps = 13320, //trp
+    .tras_ps = 32000, //tras
+    .trc_ps = 45320, //tras + trp
+    .twr_ps = 15000, //twr
+    .trfc1_ps = 260000, //trfc1
+    .trfc2_ps = 160000, //trfc2
+    .trfc4_ps = 110000, //trfc4
+    .tfaw_ps = 21000, //tfaw
+    .trrds_ps = 3300, //trrds
+    .trrdl_ps = 4900, //trrdl
+    .tccdl_ps = 5000, //tccdl
+    .refresh_rate_ps = 7800000, //refi
      .rc = 0x1f,
};

Did I miss something or change it wrong?

0 Kudos
Reply
21,069 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello hakjun oh,

You could use QCVS DDRv tool to validate and optimize DDR controller initialization parameters.

Would you please try your new generated ATF image on LS1043ARDB to check whether you encounter similar problem as booting from RGW?

Thanks,

Yiping

0 Kudos
Reply
21,069 Views
hakjunoh
Contributor III

Hi Yiping.

Are you trying to boot an ATF image for RGW into RDB?
This is the RDB log in the table above, but DDR_DEBUG option enabled, it looks like this:

RDB log with DDR_DEBUG

픭?NFO: RCW BOOT SRC is SD/EMMC
INFO: RCW BOOT SRC is SD/EMMC
INFO: esdhc_emmc_init
INFO: Card detected successfully
INFO: init done:
INFO: platform clock 300000000
INFO: DDR PLL1 1600000000
INFO: DDR PLL2 0
INFO: time base 37 ms
INFO: Parse DIMM SPD(s)
INFO: cal cs
INFO: cs_in_use = 1
INFO: cs_on_dimm[0] = 1
NOTICE: Fixed DDR on board
INFO: Time after parsing SPD 13 ms
INFO: Synthesize configurations
INFO: cs 0
INFO: odt_rd_cfg 0x0
INFO: odt_wr_cfg 0x4
INFO: odt_rtt_norm 0x3
INFO: odt_rtt_wr 0x0
INFO: auto_precharge 0
INFO: cs 1
INFO: odt_rd_cfg 0x0
INFO: odt_wr_cfg 0x0
INFO: odt_rtt_norm 0x0
INFO: odt_rtt_wr 0x0
INFO: auto_precharge 0
INFO: cs 2
INFO: odt_rd_cfg 0x0
INFO: odt_wr_cfg 0x0
INFO: odt_rtt_norm 0x0
INFO: odt_rtt_wr 0x0
INFO: auto_precharge 0
INFO: cs 3
INFO: odt_rd_cfg 0x0
INFO: odt_wr_cfg 0x0
INFO: odt_rtt_norm 0x0
INFO: odt_rtt_wr 0x0
INFO: auto_precharge 0
INFO: ctlr_init_ecc 0
INFO: x4_en 0
INFO: ap_en 0
INFO: ctlr_intlv 0
INFO: ctlr_intlv_mode 0
INFO: ba_intlv 0x0
INFO: data_bus_used 1
INFO: otf_burst_chop_en 0
INFO: burst_length 0x8
INFO: dbw_cap_shift 0
INFO: Assign binding addresses
INFO: ctlr_intlv 0
INFO: rank density 0x80000000
INFO: CS 0
INFO: base_addr 0x0
INFO: size 0x80000000
INFO: base 0x0
INFO: Total mem by assignment is 0x80000000
INFO: Calculate controller registers
INFO: Skip CL mask for this speed 0x400
INFO: Skip caslat 0x400
INFO: cs_in_use = 0x1
INFO: cs0
INFO: _config = 0x80040322
INFO: cs[0].bnds = 0x7f
INFO: sdram_cfg[0] = 0xc50c0000
INFO: sdram_cfg[1] = 0x401100
INFO: sdram_cfg[2] = 0x0
INFO: timing_cfg[0] = 0x91550018
INFO: timing_cfg[1] = 0xbab48c42
INFO: timing_cfg[2] = 0x48c111
INFO: timing_cfg[3] = 0x10c1000
INFO: timing_cfg[4] = 0x2
INFO: timing_cfg[5] = 0x3401400
INFO: timing_cfg[6] = 0x0
INFO: timing_cfg[7] = 0x13300000
INFO: timing_cfg[8] = 0x2114600
INFO: timing_cfg[9] = 0x0
INFO: dq_map[0] = 0x0
INFO: dq_map[1] = 0x0
INFO: dq_map[2] = 0x0
INFO: dq_map[3] = 0x0
INFO: sdram_mode[0] = 0x3010210
INFO: sdram_mode[1] = 0x0
INFO: sdram_mode[9] = 0x4000000
INFO: sdram_mode[8] = 0x500
INFO: sdram_mode[2] = 0x10210
INFO: sdram_mode[3] = 0x0
INFO: sdram_mode[10] = 0x400
INFO: sdram_mode[11] = 0x4000000
INFO: sdram_mode[4] = 0x10210
INFO: sdram_mode[5] = 0x0
INFO: sdram_mode[12] = 0x400
INFO: sdram_mode[13] = 0x4000000
INFO: sdram_mode[6] = 0x10210
INFO: sdram_mode[7] = 0x0
INFO: sdram_mode[14] = 0x400
INFO: sdram_mode[15] = 0x4000000
INFO: interval = 0x18600618
INFO: zq_cntl = 0x8a090705
INFO: ddr_sr_cntr = 0x0
INFO: clk_cntl = 0x3000000
INFO: cdr[0] = 0x80040000
INFO: cdr[1] = 0xa181
INFO: wrlvl_cntl[0] = 0x8675f607
INFO: wrlvl_cntl[1] = 0x7090807
INFO: wrlvl_cntl[2] = 0x7070707
INFO: debug[28] = 0x46
INFO: Time before programming controller 267 ms
INFO: Program controller registers
INFO: Reading debug[9] as 0x1f001d00
INFO: Reading debug[10] as 0x22002000
INFO: cpo_min 0x1d
INFO: cpo_max 0x22
INFO: debug[28] 0x700046
INFO: Optimal cpo_sample 0x46
INFO: *0x1080000 = 0x7f
INFO: *0x1080080 = 0x80040322
INFO: *0x1080100 = 0x10c1000
INFO: *0x1080104 = 0x91550018
INFO: *0x1080108 = 0xbab48c42
INFO: *0x108010c = 0x48c111
INFO: *0x1080110 = 0xc50c0000
INFO: *0x1080114 = 0x401100
INFO: *0x1080118 = 0x3010210
INFO: *0x1080120 = 0x600041f
INFO: *0x1080124 = 0x18600618
INFO: *0x1080128 = 0xdeadbeef
INFO: *0x1080130 = 0x3000000
INFO: *0x1080160 = 0x2
INFO: *0x1080164 = 0x3401400
INFO: *0x108016c = 0x13300000
INFO: *0x1080170 = 0x8a090705
INFO: *0x1080174 = 0xc675f607
INFO: *0x1080190 = 0x7090807
INFO: *0x1080194 = 0x7070707
INFO: *0x1080200 = 0x10210
INFO: *0x1080208 = 0x10210
INFO: *0x1080210 = 0x10210
INFO: *0x1080220 = 0x500
INFO: *0x1080224 = 0x4000000
INFO: *0x1080228 = 0x400
INFO: *0x108022c = 0x4000000
INFO: *0x1080230 = 0x400
INFO: *0x1080234 = 0x4000000
INFO: *0x1080238 = 0x400
INFO: *0x108023c = 0x4000000
INFO: *0x1080250 = 0x2114600
INFO: *0x1080280 = 0xeeeeee06
INFO: *0x1080284 = 0x11111111
INFO: *0x1080288 = 0xffffff10
INFO: *0x108028c = 0xff
INFO: *0x1080290 = 0xffff0001
INFO: *0x1080b20 = 0x8080
INFO: *0x1080b24 = 0x80000000
INFO: *0x1080b28 = 0x80040000
INFO: *0x1080b2c = 0xa181
INFO: *0x1080bf8 = 0x20501
INFO: *0x1080bfc = 0x200
INFO: *0x1080f04 = 0x2
INFO: *0x1080f08 = 0xb
INFO: *0x1080f0c = 0x14000c20
INFO: *0x1080f24 = 0x1f001d00
INFO: *0x1080f28 = 0x22002000
INFO: *0x1080f34 = 0x5000
INFO: *0x1080f48 = 0x1
INFO: *0x1080f4c = 0x94000000
INFO: *0x1080f50 = 0xf000e00
INFO: *0x1080f54 = 0x12001100
INFO: *0x1080f58 = 0xe000e00
INFO: *0x1080f5c = 0xe000e00
INFO: *0x1080f60 = 0xe000000
INFO: *0x1080f70 = 0x700046
INFO: *0x1080f9c = 0x13001300
INFO: *0x1080fa0 = 0x13001300
INFO: *0x1080fb0 = 0x3
INFO: *0x1080fb4 = 0xf0f0e10
INFO: *0x1080fb8 = 0xf0f0e0e
INFO: *0x1080fbc = 0xf0f0e10
INFO: *0x1080fc0 = 0xf0f0f0f
INFO: *0x1080fc4 = 0xf0f0f11
INFO: *0x1080fc8 = 0xf100f0f
INFO: *0x1080fcc = 0xf0e0e10
INFO: *0x1080fd0 = 0xf100f0f
INFO: *0x1080fd4 = 0xf0f0f0f
INFO: *0x1080fd8 = 0xf0f0f0f
INFO: *0x1080fdc = 0xf0f0f0f
INFO: *0x1080fe0 = 0xf0f0f0f
INFO: *0x1080fe4 = 0xf0f0f0f
INFO: *0x1080fe8 = 0xf0f0f0f
INFO: *0x1080fec = 0xf0f0f0f
INFO: *0x1080ff0 = 0xf0f0f0f
INFO: *0x1080ff4 = 0xf0f0f0f
INFO: *0x1080ff8 = 0xf0f0f0f

NOTICE: 2 GB DDR4, 32-bit, CL=11, ECC off
INFO: Time used by DDR driver 516 ms
NOTICE: BL2: v1.5(debug):LSDK-20.04
NOTICE: BL2: Built : 01:45:57, May 29 2020
INFO: Configuring TZASC-380
INFO: BL2: Doing platform setup
INFO: BL2: Loading image id 3
INFO: sd-mmc read done.
INFO: sd-mmc read done.
INFO: sd-mmc read done.
INFO: Loading image id=3 at address 0xfbe00000
INFO: sd-mmc read done.
INFO: Image id=3 loaded: 0xfbe00000 - 0xfbe0d644
INFO: BL2: Loading image id 5
INFO: sd-mmc read done.
INFO: sd-mmc read done.
INFO: sd-mmc read done.
INFO: sd-mmc read done.
INFO: sd-mmc read done.
INFO: Loading image id=5 at address 0x82000000
INFO: sd-mmc read done.
INFO: Image id=5 loaded: 0x82000000 - 0x820b886f
NOTICE: BL2: Booting BL31
INFO: Entry point address = 0xfbe00000
INFO: SPSR = 0x3cd
NOTICE: BL31: v1.5(debug):LSDK-20.04
NOTICE: BL31: Built : 01:45:52, May 29 2020
NOTICE: Welcome to LS1043 BL31 Phase
INFO: ARM GICv2 driver initialized
INFO: BL31: Initializing runtime services
WARNING: BL31: cortex_a53: CPU workaround for 835769 was missing!
WARNING: BL31: cortex_a53: CPU workaround for 843419 was missing!
INFO: BL31: cortex_a53: CPU workaround for 855873 was applied
INFO: BL31: Preparing for EL3 exit to normal world
INFO: Entry point address = 0x82000000
INFO: SPSR = 0x3c9


U-Boot 2019.10 (May 29 2020 - 02:11:12 +0100)

SoC: LS1043AE Rev1.1 (0x87920011)
Clock Configuration:
CPU0(A53):1600 MHz CPU1(A53):1600 MHz CPU2(A53):1600 MHz
CPU3(A53):1600 MHz
Bus: 300 MHz DDR: 1600 MT/s FMAN: 600 MHz
Reset Configuration Word (RCW):
00000000: 06100010 0c000000 00000000 00000000
00000010: 14550002 80004002 60106000 c1002000
00000020: 00000000 00000000 00000000 01030940
00000030: 00000000 00003004 00000096 00000001
Model: LS1043A RGW Board
Board: LS1043ARGW, boot from SD
Invalid setting
SERDES Reference Clocks:
SD1_CLK1 = 156.25MHZ, SD1_CLK2 = 100.00MHZ
DRAM: 1.9 GiB (DDR4, 32-bit, CL=11, ECC off)
Using SERDES1 Protocol: 5205 (0x1455)
SEC0: RNG instantiated
Flash: 128 MiB
NAND: 512 MiB
MMC: FSL_SDHC: 0
Loading Environment from MMC... *** Warning - bad CRC, using default environment

EEPROM: NXID v1
In: serial
Out: serial
Err: serial
Net:
MMC read: dev # 0, block # 18432, count 128 ...
Fman1: Data at 00000000f7a38f60 is not a firmware
PCIe0: pcie@3400000 disabled
PCIe1: pcie@3500000 Root Complex: no link
PCIe2: pcie@3600000 Root Complex: no link
No ethernet found.
Hit any key to stop autoboot: 0

Thanks,

hakjun oh

0 Kudos
Reply
21,069 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello hakjun oh,

Please apply your DDR patch for LS1043ARGW  on packages/firmware/atf/plat/nxp/soc-ls1043/ls1043ardb/ddr_init.c in ATF source code, then move build/firmware/atf/ and build/firmware/u-boot/, rebuild ATF image for LS1043ARDB and verify it on LS1043ARDB.

Thanks,

Yiping

0 Kudos
Reply
21,069 Views
hakjunoh
Contributor III

Hi Yiping.

Is there anything else I can do?

Thanks,

hakjun oh

0 Kudos
Reply
21,069 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello hakjun oh,

Please check whether RCW for LS1043ARGW is correct. 

Do you have CodeWarrior and CodeWarrior TAP? If yes, please create a bareboard project in CodeWarrior and check whether the sample project can run on the target board. In CodeWarrior initialization file, please modify DDR initialization parameters with your debug data, please use USE_SAFE_RCW = True in CW initialization file to use the hard-coded RCW.

Thanks,

Yiping

0 Kudos
Reply
21,069 Views
hakjunoh
Contributor III

Hi Yiping.

Yes. The bare board project worked fine.

I think there perhaps have problem with RCW so I modified ASK's RCW to work with SDHC and booted, but the result is the same.

What shall we do next?

Reset Configuration Word (RCW):
00000000: 08100010 0a000000 00000000 00000000
00000010: 14550002 80004002 60106000 c1002000
00000020: 00000000 00000000 00000000 01030940
00000030: 00000000 00003004 00000096 00000001

Thanks,

hakjun oh

0 Kudos
Reply
21,069 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello hakjun oh,

In CodeWarrior initialization file, please configure USE_SAFE_RCW = False, please configure the target board as booting from SD card, then try whether the bareboard project can work fine.

Thanks,

Yiping

0 Kudos
Reply
21,069 Views
hakjunoh
Contributor III

Hi Yiping.

Oops, sorry. I didn't understand the prev answer to the question well.

In the previous question, RGW booting with the USE_SAFE_RCW = True option causes the machine to hang.

RGW booted with SAFE_RCW
INFO: RCW BOOT SRC is SD/EMMC
INFO: RCW BOOT SRC is SD/EMMC
INFO: esdhc_emmc_init
INFO: Card detected successfully
INFO: init done:
INFO: platform clock 400000000
INFO: DDR PLL1 1600000000
INFO: DDR PLL2 0
INFO: time base 32 ms
INFO: Parse DIMM SPD(s)
INFO: cal cs
INFO: cs_in_use = 1
INFO: cs_on_dimm[0] = 1
NOTICE: Fixed DDR on board
INFO: Time after p

And when the diagnosis starts, an error is displayed in 2 items.

Test NameInfo
......
Run target initialization scriptDDR: initialization failed (ERR_DETECT = 0x00000080).
Test DDR memory accessMemory verification failed. First mismatch was found at address 0x80000000. Expected 'aa', but found '55'.
......

But likewise, booting the RDB with the USE_SAFE_RCW = True option cause hang.

RDB booted with SAFE_RCW
INFO: RCW BOOT SRC is SD/EMMC
INFO: RCW BOOT SRC is SD/EMMC
INFO: esdhc_emmc_init
INFO: Card detected successfully
INFO: init done:
INFO: platform clock 400000000
INFO: DDR PLL1 1600000000
INFO: DDR PLL2 0
INFO: time base 32 ms
INFO: Parse DIMM SPD(s)
INFO: cal cs
INFO: cs_in_use = 1
INFO: cs_on_dimm[0] = 1
NOTI

However, the diagnosis has not error.

Thanks,

hakjun oh

0 Kudos
Reply
21,069 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please use DDRv to connect your custom board to optimize and validate your DDR configuration parameters on the custom board.

0 Kudos
Reply
21,069 Views
hakjunoh
Contributor III

Hi Yiping.

I found something while I was looking at the board. I thought it was MT40A512M88HX-093E because it was written as MT40A512M8HX-093E in the RDB source and schematic. However, I confirmed that the FBGA codes of RDB and RGW are the same.

Different results were obtained when the Validation Test was performed by matching the set values using Codewarrior DDRv. In RDB, all tests are Passed, but in RGW, all tests are Failed.

RGW DDRRDB DDR
RGW_DDR_CODE.jpgRDB_DDR_CODE.jpg
RGW-DDR_VAL.pngRDB-DDR_VAL.png

The more I do, the more I can't figure out the cause. What more should I do?

I will continue to validate DDR configuration parameters.

Thanks,

hakjun oh

0 Kudos
Reply
21,069 Views
hakjunoh
Contributor III

Yiping.

I found reason of failed DDR validation in Codewarrior DDRv. It should have set DQ values. I didn't know if there was this option.
Either way, the results are good. Now I should check if there is any DQ setting in the ATF source.

RGW DDR Validation
RGW-DDR_VAL-PASS.png

Thanks,

hakjun oh

0 Kudos
Reply
21,069 Views
hakjunoh
Contributor III

Hi Yiping.

The problem has been resolved.

plat/nxp/soc-ls1043/ls1043ardb/ddr_init.c

diff --git a/plat/nxp/soc-ls1043/ls1043ardb/ddr_init.c b/plat/nxp/soc-ls1043/ls1043ardb/ddr_init.c
index 705adb014..776204d57 100644
--- a/plat/nxp/soc-ls1043/ls1043ardb/ddr_init.c
+++ b/plat/nxp/soc-ls1043/ls1043ardb/ddr_init.c
@@ -92,33 +92,33 @@ int ddr_board_options(struct ddr_info *priv)
      return 0;
}

 

/* DDR model number: MT40A512M8HX-093E */
struct dimm_params ddr_raw_timing = {
      .n_ranks = 1,
      .rank_density = 2147483648u,
      .capacity = 2147483648u,
      .primary_sdram_width = 32,
      .n_row_addr = 15,
      .n_col_addr = 10,
      .bank_group_bits = 2,
      .burst_lengths_bitmask = 0x0c,
      .tckmin_x_ps = 938,
      .tckmax_ps = 1500,
      .caslat_x = 0x000DFA00,
      .taa_ps = 13500,
      .trcd_ps = 13500,
      .trp_ps = 13500,
      .tras_ps = 33000,
      .trc_ps = 46500,
      .twr_ps = 15000,
      .trfc1_ps = 260000,
      .trfc2_ps = 160000,
      .trfc4_ps = 110000,
      .tfaw_ps = 21000,
      .trrds_ps = 3700,
      .trrdl_ps = 5300,
      .tccdl_ps = 5355,
      .refresh_rate_ps = 7800000,
+    .dq_mapping[0] = 0x15,
+    .dq_mapping[1] = 0x36,
+    .dq_mapping[2] = 0x15,
+    .dq_mapping[3] = 0x35,
+    .dq_mapping[4] = 0x15,
+    .dq_mapping[5] = 0x36,
+    .dq_mapping[6] = 0x16,
+    .dq_mapping[7] = 0x36,
+    .dq_mapping[8] = 0x1,
+    .dq_mapping[9] = 0x21,
+    .dq_mapping[10] = 0x0,
+    .dq_mapping[11] = 0x0,
+    .dq_mapping[12] = 0x0,
+    .dq_mapping[13] = 0x0,
+    .dq_mapping[14] = 0x0,
+    .dq_mapping[15] = 0x0,
+    .dq_mapping[16] = 0x0,
+    .dq_mapping[17] = 0x0,
+    .dq_mapping_ors = 0,
      .rc = 0x1f,
};

 

Thank you very much.

hakjun oh

14,041 Views
ChienNQ
Contributor II

Dear Hakjunoh, 

I have same problem. Can you share me how to mapping data? 

Thanks so much!

0 Kudos
Reply
21,069 Views
hakjunoh
Contributor III

Hi Yiping.

I'm not sure what I understand, but DDR patch for LS1043ARGW applied to flexbuilder. And rebuilded u-boot and atf.

The rebuilt image was written to SD and booted from LS1043ARDB.

The boot log is:

Boot log on LS1043ARDB with DDR patch applied.

NOTICE: Fixed DDR on board

NOTICE: 2 GB DDR4, 32-bit, CL=11, ECC off
NOTICE: BL2: v1.5(release):LSDK-20.04
NOTICE: BL2: Built : 15:22:06, Jun 1 2020
NOTICE: BL31: v1.5(release):LSDK-20.04
NOTICE: BL31: Built : 15:22:10, Jun 1 2020
NOTICE: Welcome to LS1043 BL31 Phase


U-Boot 2019.10-dirty (Jun 01 2020 - 15:12:34 +0900)

SoC: LS1043AE Rev1.1 (0x87920011)
Clock Configuration:
CPU0(A53):1600 MHz CPU1(A53):1600 MHz CPU2(A53):1600 MHz
CPU3(A53):1600 MHz
Bus: 300 MHz DDR: 1600 MT/s FMAN: 600 MHz
Reset Configuration Word (RCW):
00000000: 06100010 0c000000 00000000 00000000
00000010: 14550002 80004002 60106000 c1002000
00000020: 00000000 00000000 00000000 01030940
00000030: 00000000 00003004 00000096 00000001
Model: LS1043A RDB Board
Board: LS1043ARGW, boot from SD
Invalid setting
SERDES Reference Clocks:
SD1_CLK1 = 156.25MHZ, SD1_CLK2 = 100.00MHZ
DRAM: 1.9 GiB (DDR4, 32-bit, CL=11, ECC off)
Using SERDES1 Protocol: 5205 (0x1455)
SEC0: RNG instantiated
FSL_SDHC: 0

MMC read: dev # 0, block # 18944, count 128 ...
Not a microcode
Flash: 128 MiB
NAND: 512 MiB
MMC: Loading Environment from MMC... *** Warning - bad CRC, using default environment

EEPROM: NXID v1
In: serial
Out: serial
Err: serial
Net:
MMC read: dev # 0, block # 18432, count 128 ...
Fman1: Data at 00000000f7a380b0 is not a firmware
PCIe0: pcie@3400000 disabled
PCIe1: pcie@3500000 Root Complex: no link
PCIe2: pcie@3600000 Root Complex: no link
No ethernet found.
Hit any key to stop autoboot: 10

Thanks,

hakjun oh

0 Kudos
Reply