[LS1043ARDB] Cores boot at different exception levels

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[LS1043ARDB] Cores boot at different exception levels

Jump to solution
1,844 Views
zalbassam
Contributor I

Hi,

Iam having a problem with one of the LS1043ARDB board (Orange box), after U-boot loads my program, core0 is at exception level 2 (EL2), but the other cores boot at EL1 and get hang when trying to switch to EL2. I have another LS1043ARDB board (Gray box) and all the cores boot at EL2. the same uboot image is on both boards: "U-Boot 2016.012.0+ga9b437f (May 15 2016 - 11:01:10 +0800)", and both boards have the same dip switch settings. I have however noticed the below differences in the uboot boot log:

The orange box (not working):

CPLD:  V1.4

PPA Firmware: Version 0.1

EEPROM: NXID v1

The gray box (working):

CPLD:  V1.5

PPA Firmware: Version 0.2

EEPROM: Invalid ID (0b 0c 03 04)

Any idea why the orange box has the cores boot at different EL? Should  the color of the box mean something (like secure)?

Thanks,

Labels (1)
0 Kudos
Reply
1 Solution
1,662 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Zaid Albassam,

The problem should be caused by PPA firmware not compatible with U-BOOT 2016.012.

Please flash the attached ppa image on the problem board.

PPA address on NOR flash of LS1043.

bank 0:0x60500000

bank 4: 0x64500000


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,663 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Zaid Albassam,

The problem should be caused by PPA firmware not compatible with U-BOOT 2016.012.

Please flash the attached ppa image on the problem board.

PPA address on NOR flash of LS1043.

bank 0:0x60500000

bank 4: 0x64500000


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,662 Views
zalbassam
Contributor I

Hi yipingwang‌,

My board now shows that the PPA version is upped to v0.2, and with that my problem is resolved.

I wished that U-boot could detect these incompatibility with the PPA and at least print a warning in the boot log, It could have saved me couple of days of investigations.

Anyways, thanks for the help.

Zaid

0 Kudos
Reply