How To flash fresh FRDM-LS1012A with empty flash?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How To flash fresh FRDM-LS1012A with empty flash?

3,251 Views
shyam_baldha
Fresh Out Contributor

Hello Community,

1. How to Flash fresh FRDM-LS1012A board which is not having any binaries (RCW, U-BOOT, KERNAL IMAGE)?     Exactly what are the tools needed and what procedure to follow?

2. Can some one point me to the documents, for how to use below listed tool for FRDM-LS1012A board:

         - Code warrior 

         - Code warrior - TAP

         - QCVS 

3. Which tool is to be used for flashing CMSIS-DAP binary? and Information/documents to use that tool.

Thanks,

Shyam

Labels (1)
Tags (1)
0 Kudos
Reply
5 Replies

2,891 Views
ufedor
NXP Employee
NXP Employee

Which exactly board is in question?

0 Kudos
Reply

2,891 Views
shyam_baldha
Fresh Out Contributor

LS1012A freedom board.

0 Kudos
Reply

2,891 Views
ufedor
NXP Employee
NXP Employee

Why it is "fresh"?

It has to be fully programmed during manufacturing.

0 Kudos
Reply

2,891 Views
shyam_baldha
Fresh Out Contributor

We are Designing a customized board by taking reference of FRDM-LS1012A board with some few changes.  So I need to do all booting processes to bring-up custom board which having empty flash. 

0 Kudos
Reply

2,891 Views
ufedor
NXP Employee
NXP Employee

Please create a Technical Case for each of the numbered sections - refer to the following link:

https://community.freescale.com/thread/381898

0 Kudos
Reply