LS1043AQDS: u-boot binary

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043AQDS: u-boot binary

2,439件の閲覧回数
carlos-m-ribeiro
Contributor I

Hello,

Which flags/defconfig/configurations/files we need to compile and generate the u-boot binary spl-pbl (with rcw) to ls1043 qspi?

Best regards

0 件の賞賛
返信
5 返答(返信)

2,428件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

It is impossible to get QSPI u-boot binary image with RCW by compiling u-boot source code.

You could download flexbuild_lsdk2012, run command "$ flex-builder -c rcw -m ls1046aqds" to get QSPI RCW binary file rcw_1600_qspiboot.bin.swapped in packages/firmware/rcw/ls1046aqds/RR_FFSNPPPH_1133_5559/. Please deploy RCW at 0x00000000, u-boot at 0x00100000 on QSPI flash

0 件の賞賛
返信

2,420件の閲覧回数
carlos-m-ribeiro
Contributor I

Thank you again, but you refer ls1046aqds, it is the same for ls1023/ls1043 (quad-core version)?

 

Best regards

0 件の賞賛
返信

2,402件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

You could download flexbuild_lsdk2012, run command "$flex-builder -c rcw -m ls1043aqds" to get QSPI RCW binary file rcw_1600_qspiboot.bin.swapped in packages/firmware/rcw/ls1043aqds/RR_FQPP_1455/. Please deploy RCW at 0x00000000, u-boot at 0x00100000 on QSPI flash

0 件の賞賛
返信

2,437件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please compile QSPI u-boot for ls1043aqds with configure file "ls1043aqds_qspi_defconfig" in u-boot source code. The generated u-boot image doesn't include RCW.

0 件の賞賛
返信

2,433件の閲覧回数
carlos-m-ribeiro
Contributor I

Thank you for your response but how I can include RCW in u-boot binary with qpsi via menuconfig?

Best regards

0 件の賞賛
返信