[LS1043A] Verify ITS Fuse state

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[LS1043A] Verify ITS Fuse state

1,164 Views
samfuxu
Contributor I

Hello,

I'm trying to verify the state of the Intent To Secure fuse on LS1023A and LS1043A based boards.

After provisioning the fuse configuration and U-Boot image (which does not give any command line interface to the user), how can I verify the state of the fuses and in particular the ITS fuse ? Is it feasible via JTAG ?

0 Kudos
Reply
3 Replies

748 Views
samfuxu
Contributor I

Hello @SebastianG 

Do you have any update on this topic?

Which procedure can follow to verify ITS status via JTAG?

I am looking to something similar to: https://community.nxp.com/t5/Layerscape/How-to-detect-if-device-was-fused-secure-boot/m-p/1314528

Thank you,

Regars

 

0 Kudos
Reply

1,116 Views
SebastianG
NXP TechSupport
NXP TechSupport

Hi @samfuxu,

Regarding to the question " Is it feasible via JTAG ?"

Yes, is feasible via JTAG

0 Kudos
Reply

1,133 Views
SebastianG
NXP TechSupport
NXP TechSupport

Hello @samfuxu,

I'm working on your question, When I have any update I will let you know

Regards

0 Kudos
Reply