LS1043A SATA IO Errors...

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043A SATA IO Errors...

1,767 Views
edwardchoi
Contributor II

I've recently staretd seeing the following errors, with the sata attached on our LS1043A custom board.

There has been no problem with ourhardware when running LSDK 18.04 (Ununtu 18.04 /w linux 4.6.79).

But, LS1043A board failed to initialize SATA SSD when running LSDK 21.08  (Ununtu 20.04 /w linux 5.10.35).

 

<< Kernle log >>

root@localhost:/home/wbpa/workspace/sh# dmesg
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000] Linux version 5.10.35-dirty (edchoi@crztech-HP-ProDesk-400-G7-Microtower-PC) (aarch64-linux-gnu-gcc (Ubuntu 9.4.0-1ubuntu1~20.04.2) 9.4.0, GNU ld (GNU Binutils for Ubuntu) 2.34) #1 SMP PREEMPT Thu Nov 2 16:22:21 KST 2023
[ 0.000000] Machine model: LS1043A RDB Board

.................................

[ 8.926884] ata1: SATA link up 6.0 Gbps (SStatus 133 SControl 300)
[ 8.933464] ata1.00: configured for UDMA/133
[ 8.937851] sd 0:0:0:0: [sda] tag#11 UNKNOWN(0x2003) Result: hostbyte=0x00 driverbyte=0x08 cmd_age=0s
[ 8.947103] sd 0:0:0:0: [sda] tag#11 Sense Key : 0x5 [current]
[ 8.953031] sd 0:0:0:0: [sda] tag#11 ASC=0x21 ASCQ=0x4
[ 8.958270] sd 0:0:0:0: [sda] tag#11 CDB: opcode=0x28 28 00 00 00 08 80 00 00 08 00
[ 8.965948] blk_update_request: I/O error, dev sda, sector 2176 op 0x0:(READ) flags 0x80700 phys_seg 1 prio class 0
[ 8.976421] ata1: EH complete
[ 9.026846] ata1.00: exception Emask 0x12 SAct 0x4 SErr 0x380500 action 0x6 frozen
[ 9.034484] ata1.00: irq_stat 0x08000000, interface fatal error
[ 9.040421] ata1: SError: { UnrecovData Proto 10B8B Dispar BadCRC }
[ 9.046694] ata1.00: failed command: READ FPDMA QUEUED
[ 9.051849] ata1.00: cmd 60/f8:10:08:09:00/00:00:00:00:00/40 tag 2 ncq dma 126976 in
res 40/00:14:08:09:00/00:00:00:00:00/40 Emask 0x12 (ATA bus error)
[ 9.067597] ata1.00: status: { DRDY }
[ 9.071267] ata1: hard resetting link
[ 9.550844] ata1: SATA link up 6.0 Gbps (SStatus 133 SControl 300)
[ 9.557388] ata1.00: configured for UDMA/133
[ 9.561772] sd 0:0:0:0: [sda] tag#2 UNKNOWN(0x2003) Result: hostbyte=0x00 driverbyte=0x08 cmd_age=0s
[ 9.570929] sd 0:0:0:0: [sda] tag#2 Sense Key : 0x5 [current]
[ 9.576768] sd 0:0:0:0: [sda] tag#2 ASC=0x21 ASCQ=0x4
[ 9.581927] sd 0:0:0:0: [sda] tag#2 CDB: opcode=0x28 28 00 00 00 09 08 00 00 f8 00
[ 9.589511] blk_update_request: I/O error, dev sda, sector 2312 op 0x0:(READ) flags 0x80700 phys_seg 31 prio class 0
[ 9.600072] ata1: EH complete
[ 11.886854] ata1: limiting SATA link speed to 3.0 Gbps
[ 11.886868] ata1.00: exception Emask 0x12 SAct 0x35840c SErr 0x380500 action 0x6 frozen
[ 11.895397] ata1.00: irq_stat 0x08000000, interface fatal error
[ 11.902496] ata1: SError: { UnrecovData Proto 10B8B Dispar BadCRC }
[ 11.909386] ata1.00: failed command: READ FPDMA QUEUED
[ 11.915620] ata1.00: cmd 60/08:10:70:0f:00/00:00:00:00:00/40 tag 2 ncq dma 4096 in
res 40/00:1c:78:0f:00/00:00:00:00:00/40 Emask 0x12 (ATA bus error)
[ 11.931992] ata1.00: status: { DRDY }

.............................

[ 12.146959] ata1: hard resetting link
[ 12.282635] EXT4-fs (sdb1): mounted filesystem with ordered data mode. Opts: (null)
[ 12.622853] ata1: SATA link up 3.0 Gbps (SStatus 123 SControl 320)
[ 12.623104] ata1.00: configured for UDMA/133
[ 12.623221] sd 0:0:0:0: [sda] tag#2 UNKNOWN(0x2003) Result: hostbyte=0x00 driverbyte=0x08 cmd_age=0s
[ 12.623229] sd 0:0:0:0: [sda] tag#2 Sense Key : 0x5 [current]
[ 12.623234] sd 0:0:0:0: [sda] tag#2 ASC=0x21 ASCQ=0x4
[ 12.623241] sd 0:0:0:0: [sda] tag#2 CDB: opcode=0x28 28 00 00 00 0f 70 00 00 08 00
[ 12.623247] blk_update_request: I/O error, dev sda, sector 3952 op 0x0:(READ) flags 0x80700 phys_seg 1 prio class 0
[ 12.633830] sd 0:0:0:0: [sda] tag#3 UNKNOWN(0x2003) Result: hostbyte=0x00 driverbyte=0x08 cmd_age=0s
[ 12.633838] sd 0:0:0:0: [sda] tag#3 Sense Key : 0x5 [current]
[ 12.633843] sd 0:0:0:0: [sda] tag#3 ASC=0x21 ASCQ=0x4
[ 12.633850] sd 0:0:0:0: [sda] tag#3 CDB: opcode=0x28 28 00 00 00 0f 78 00 00 08 00
[ 12.633856] blk_update_request: I/O error, dev sda, sector 3960 op 0x0:(READ) flags 0x80700 phys_seg 1 prio class 0

...................

 

< smartctl result >

edwardchoi_0-1725871897298.png

 

0 Kudos
Reply
1 Reply

1,720 Views
Oswalag
NXP TechSupport
NXP TechSupport

Please review if your RCW is the same for both software version and check if the Compile-time Configuration Options are marked as "yes".

You can also try to upgrade to the latest LLDP version with kernel 6.1 https://www.nxp.com/design/design-center/software/embedded-software/linux-software-and-development-t...

https://www.nxp.com/docs/en/user-guide/UG10081_LLDP_6.1.55_2.2.0.pdf

 

0 Kudos
Reply