Without SEC enabled, is Secure Boot possible with the LS1021A?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Without SEC enabled, is Secure Boot possible with the LS1021A?

1,629 次查看
Karlito
Contributor I

Hi, I am currently using an NXP ls1021A and would like to implement Secure Boot. Is this possible without the Security Engine (SEC) enabled? Or is the implementation of Secure Boot only possible in combination with the use of the Security Engine?

@Layerscape® 1021A | NXP Semiconductors

0 项奖励
回复
2 回复数

1,618 次查看
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

SEC disabled Layerscape chips cannot perform secure boot, the security engine (SEC 5.5) is designed to support Secure Boot.

Have a nice day!

Oswaldo.

 

0 项奖励
回复

1,316 次查看
Karlito
Contributor I

Thank you for your reply. Where can I find information on implementing Secure Boot with the LS1021A? Is there a step-by-step guide? I also want to know what is part of the SEC? Is the SFP module part of the SEC? Thanks in advance.

LS1021A 

标记 (2)
0 项奖励
回复