LS1043A QUICC engine microcode TDM peripheral usage documentation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043A QUICC engine microcode TDM peripheral usage documentation

1,812 Views
1271792207
Contributor II

Hello,

I am currently using TDM inside the LS1043A chip, which is based on QE.

Can anybody please let me know :

1. Initialization steps for QE on LS1043 

3. Is there any application note ? I am planning to use QUICC Engine TDM interface.

Labels (1)
1 Reply

1,678 Views
Pavel
NXP Employee
NXP Employee

See the QUICC Engine Block Reference Manual with Protocol Interworking - Reference Manual (REV 9):

https://www.nxp.com/webapp/Download?colCode=QEIWRM

 

NXP offers Linux BSP for the LS1043a boards: SDK 2.0-1703 and LSDK 18.12.

These BSP supports TDM.

 

See the Section 7.12 of SDK 2.0-1703 documentation:

https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf

 

See the Section 7.2.15 of LSDK 18.12 documentation:

https://www.nxp.com/docs/en/supporting-information/LSDK-KC-REV18.12.pdf

 

These documentations contains examples for TDM initialization and testing.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------