[LS1043ARDB] full duplex mode for dspi?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[LS1043ARDB] full duplex mode for dspi?

1,400 Views
randy_wang
Contributor II

Hi,

Is the ls1043ardb dspi full duplex mode or half duplex?

and is possible to set dspi full/half duplex mode?

Thanks.

0 Kudos
Reply
1 Reply

1,349 Views
alexander_yakov
NXP Employee
NXP Employee

SPI controller is full-duplex by design - "serial data in" and "serial data out" lines are separate, so you can transmit and receive simultaneously.


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------