LS1043A PCIe End point

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1043A PCIe End point

跳至解决方案
3,414 次查看
SrinivasP
Contributor II

Can we configure PCIe of  LS1043A as End point? If yes, is it with RCW register?

标记 (1)
0 项奖励
回复
1 解答
3,410 次查看
ufedor
NXP Employee
NXP Employee

Please refer to the QorIQ LS1043A Reference Manual, 28.1 The PCI Express controller as implemented on the chip:

"NOTE
The EP mode is not supported in LS1043A; any references to that should be ignored."

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,402 次查看
SrinivasP
Contributor II

I want to get clarified on one more topic. As per PCIe spec and generation a specified transfer rate is mentioned (2. GT/s , 5 GT/s etc). Is this transfer rate fixed or can we configure any transfer rate below the maximum specified? 

0 项奖励
回复
3,411 次查看
ufedor
NXP Employee
NXP Employee

Please refer to the QorIQ LS1043A Reference Manual, 28.1 The PCI Express controller as implemented on the chip:

"NOTE
The EP mode is not supported in LS1043A; any references to that should be ignored."

0 项奖励
回复
3,405 次查看
SrinivasP
Contributor II

Thank you

0 项奖励
回复