LS1043A PCIe End point

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043A PCIe End point

Jump to solution
3,419 Views
SrinivasP
Contributor II

Can we configure PCIe of  LS1043A as End point? If yes, is it with RCW register?

Tags (1)
0 Kudos
Reply
1 Solution
3,415 Views
ufedor
NXP Employee
NXP Employee

Please refer to the QorIQ LS1043A Reference Manual, 28.1 The PCI Express controller as implemented on the chip:

"NOTE
The EP mode is not supported in LS1043A; any references to that should be ignored."

View solution in original post

0 Kudos
Reply
3 Replies
3,407 Views
SrinivasP
Contributor II

I want to get clarified on one more topic. As per PCIe spec and generation a specified transfer rate is mentioned (2. GT/s , 5 GT/s etc). Is this transfer rate fixed or can we configure any transfer rate below the maximum specified? 

0 Kudos
Reply
3,416 Views
ufedor
NXP Employee
NXP Employee

Please refer to the QorIQ LS1043A Reference Manual, 28.1 The PCI Express controller as implemented on the chip:

"NOTE
The EP mode is not supported in LS1043A; any references to that should be ignored."

0 Kudos
Reply
3,410 Views
SrinivasP
Contributor II

Thank you

0 Kudos
Reply