LS1043A DPAA debug on CodeWarrior

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043A DPAA debug on CodeWarrior

8,392件の閲覧回数
smruthi_ramesh
Contributor II

Hi, I have the DPDK driver running on the LS1043A. is there a way to debug the application via CodeWarrior? I would like to step through the code and understand how the DPAA driver works.

ラベル(1)
0 件の賞賛
返信
13 返答(返信)

8,267件の閲覧回数
hemantagrawal
NXP Employee
NXP Employee

why don't you use gdb for debugging? 

you can use gdbserver and gdb client for line by line debugging. 

0 件の賞賛
返信

8,259件の閲覧回数
smruthi_ramesh
Contributor II

Okay will try that. Thanks

0 件の賞賛
返信

8,376件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

After installing CodeWarrior for ARMv8, you could refer to section "8.2 Linux application debug" in document C:\Freescale\CW4NET_v2020.06\CW_ARMv8\ARMv8\Help\PDF\ARMv8_Targeting_Manual.pdf.

0 件の賞賛
返信

8,356件の閲覧回数
smruthi_ramesh
Contributor II

Thank you. I went through the manual, that talks about setting up a remote connection. But the board is connected via CodeWarrior TAP as USB serial port and not an IP address. What is to be done in that case?

0 件の賞賛
返信

8,335件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

In Linux application debugging, CodeWarrior TAP is not used, Ethernet is used to connect the host PC and the target board.

0 件の賞賛
返信

8,328件の閲覧回数
smruthi_ramesh
Contributor II

Okay thanks for the reply. How do I set up the ethernet connection between the board and my PC? I tried looking for it in the CodeWarrior guide, but didnt find any instructions

0 件の賞賛
返信

8,310件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the section "8.2.2.2 Updating remote connection" in the document.

Please click Run->Debug Configuration->C/C++ Remote Application->Edit

yipingwang_0-1599637943169.png

Please specify the IP address of the Linux target board, specify the user name and password to login in the target board.

0 件の賞賛
返信

8,304件の閲覧回数
smruthi_ramesh
Contributor II

Thank you. I dont know how to set up the IP address for the LS1043A board. That is what I want to ask

0 件の賞賛
返信

8,298件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

You could configure IP address on LS1043ARDB as the following

ifconfig fm1-mac1 10.171.171.10

Then try whether you could use ssh to access the target board, with the user name and password specified in CodeWarrior IDE.

0 件の賞賛
返信

8,293件の閲覧回数
smruthi_ramesh
Contributor II

I tried that and am getting the following error:

smruthi_ramesh_0-1599774403919.png

I tried to ssh into the IP address but it gave a connection timeout error.

0 件の賞賛
返信

8,289件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Which version SDK/LSDK are you using on the target board?

How do you boot up the target board? Would you please provide the whole console log booting up the target board?

 

0 件の賞賛
返信

8,284件の閲覧回数
smruthi_ramesh
Contributor II

I am using LSDK 2004. I am booting the board with an SD card that has the LSDK 2004 version

I am attaching screenshots of the boot log.

7.jpg

6.jpg

5.jpg

4.jpg

3.jpg

2.jpg

1.jpg

9.jpg

8.jpg

         

0 件の賞賛
返信

8,237件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

In USDPAA dts file fsl-ls1043a-rdb-usdpaa.dts, all Ethernet ports have been assigned to DPDK, you need to delete one Ethernet port definition in the dts file to assign it to Linux Kernel.

fsl,dpaa {
compatible = "fsl,ls1043a", "fsl,dpaa", "simple-bus";
dma-coherent;

/* ethernet@0 {
compatible = "fsl,dpa-ethernet-init";
fsl,bman-buffer-pools = <&bp7 &bp8 &bp9>;
fsl,qman-frame-queues-rx = <0x50 1 0x51 1>;
fsl,qman-frame-queues-tx = <0x70 1 0x71 1>;
};*/

... ...

 

0 件の賞賛
返信