LS1043 POWER DOWN MODE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043 POWER DOWN MODE

5,174 Views
nikhilprakash
Contributor IV

Hi,

I am currently working on LS1043ARDB reference board.I am a bit confused about the power down mode.Could anyone suggest me on how the power down mode can be set in LS1043ARDB.Also will the nand flash interface(ifc)be up at that time???Please help me.

Thanks in advance

Labels (1)
0 Kudos
Reply
10 Replies

4,863 Views
ufedor
NXP Employee
NXP Employee

1) You wrote:

> I am a bit confused about the power down mode.

Which exactly place in the board's documentation is unclear?

2) Also will the nand flash be up at that time?

NAND Flash is powered from +1_8V which is always on.

0 Kudos
Reply

4,863 Views
nikhilprakash
Contributor IV

Hi ufedor,

First of all thanks for the quick response.I am confused  on how to set the  power down mode in LS1043ARDB board.Also does that have any effect on ifc interface???Please help....

Thanks in advance

0 Kudos
Reply

4,863 Views
ufedor
NXP Employee
NXP Employee

Where exactly in the RDB documentation the power down mode is mentioned?

0 Kudos
Reply

4,863 Views
nikhilprakash
Contributor IV

Hi ufedor,

I am going through the "Run Control and Power Management"  chapter.

Thanks in advance

0 Kudos
Reply

4,863 Views
ufedor
NXP Employee
NXP Employee

Of which exactly document?

What is its name, revision?

0 Kudos
Reply

4,863 Views
nikhilprakash
Contributor IV

Hi ufedor,

Reference manual REV D and REV C.

0 Kudos
Reply

4,863 Views
ufedor
NXP Employee
NXP Employee

Excuse me, the QorIQ LS1043A Reference Manual, Rev. D, Chapter 13 Run Control and Power Management (RCPM) does not mention "power down" mode. Which exacly RM section or statement is in question?

0 Kudos
Reply

4,863 Views
nikhilprakash
Contributor IV

Hi ufedor,

Could you please suggest me on how to set power down mode in LS1043ARDB.Also could you suggest me where to refer to for this section.Please help.

0 Kudos
Reply

4,863 Views
ufedor
NXP Employee
NXP Employee

Supported power management mode is CPU Hotplug.

You can offline cpu at runtime.

/* Offline cpu */

echo 0 > /sys/devices/system/cpu/cpu#/online

Note: cpu# is the cpu number you want to offline. cpu0 could not plug off as boot core.

/* Online cpu */

echo 1 > /sys/devices/system/cpu/cpu#/online

Note: For e6500 based cores, if all cores in one cluster are offline the cluster will automatically enter PCL10 state to save more power.

0 Kudos
Reply

4,863 Views
nikhilprakash
Contributor IV

Thanks ufedor.

0 Kudos
Reply