LS1043 POWER DOWN MODE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043 POWER DOWN MODE

5,163件の閲覧回数
nikhilprakash
Contributor IV

Hi,

I am currently working on LS1043ARDB reference board.I am a bit confused about the power down mode.Could anyone suggest me on how the power down mode can be set in LS1043ARDB.Also will the nand flash interface(ifc)be up at that time???Please help me.

Thanks in advance

ラベル(1)
0 件の賞賛
返信
10 返答(返信)

4,852件の閲覧回数
ufedor
NXP Employee
NXP Employee

1) You wrote:

> I am a bit confused about the power down mode.

Which exactly place in the board's documentation is unclear?

2) Also will the nand flash be up at that time?

NAND Flash is powered from +1_8V which is always on.

0 件の賞賛
返信

4,852件の閲覧回数
nikhilprakash
Contributor IV

Hi ufedor,

First of all thanks for the quick response.I am confused  on how to set the  power down mode in LS1043ARDB board.Also does that have any effect on ifc interface???Please help....

Thanks in advance

0 件の賞賛
返信

4,852件の閲覧回数
ufedor
NXP Employee
NXP Employee

Where exactly in the RDB documentation the power down mode is mentioned?

0 件の賞賛
返信

4,852件の閲覧回数
nikhilprakash
Contributor IV

Hi ufedor,

I am going through the "Run Control and Power Management"  chapter.

Thanks in advance

0 件の賞賛
返信

4,852件の閲覧回数
ufedor
NXP Employee
NXP Employee

Of which exactly document?

What is its name, revision?

0 件の賞賛
返信

4,852件の閲覧回数
nikhilprakash
Contributor IV

Hi ufedor,

Reference manual REV D and REV C.

0 件の賞賛
返信

4,852件の閲覧回数
ufedor
NXP Employee
NXP Employee

Excuse me, the QorIQ LS1043A Reference Manual, Rev. D, Chapter 13 Run Control and Power Management (RCPM) does not mention "power down" mode. Which exacly RM section or statement is in question?

0 件の賞賛
返信

4,852件の閲覧回数
nikhilprakash
Contributor IV

Hi ufedor,

Could you please suggest me on how to set power down mode in LS1043ARDB.Also could you suggest me where to refer to for this section.Please help.

0 件の賞賛
返信

4,852件の閲覧回数
ufedor
NXP Employee
NXP Employee

Supported power management mode is CPU Hotplug.

You can offline cpu at runtime.

/* Offline cpu */

echo 0 > /sys/devices/system/cpu/cpu#/online

Note: cpu# is the cpu number you want to offline. cpu0 could not plug off as boot core.

/* Online cpu */

echo 1 > /sys/devices/system/cpu/cpu#/online

Note: For e6500 based cores, if all cores in one cluster are offline the cluster will automatically enter PCL10 state to save more power.

0 件の賞賛
返信

4,852件の閲覧回数
nikhilprakash
Contributor IV

Thanks ufedor.

0 件の賞賛
返信