Hi,
I am currently working on LS1043ardb reference board.I want to access USB2_DRVVBUS,USB2_PWRFAULT,USB3_DRVVBUS which is an alternate functionality of IIC3 and IIC4.Can anyone suggest me on how to set extended rcw pin mux register.Please help.
Thanks in advance
May be you mean what values should be set to the Extended RCW PinMux Control Register for required configuration?
It is supposed that on the LS1043ardb USB2_DRVVBUS USB2_PWRFAULT should be configured when system has started. Check SW3[7] settings (default should be 1). LS1043A I2C2, I2C3, and I2C4 are not used, to simplify the circuit and save many mux/demux parts, LS1043ARDB attach all I2C devices to I2C1 port.