LS1028A new design without CPLD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LS1028A new design without CPLD

跳至解决方案
2,011 次查看
mkraj
Contributor III

Dear NXP expert

We are planning to go for a new LS1028A based board design without CPLD. We want to implement all reset and control outside CPLD.

Is there any dependency on firmware? Is it mandatory to use CPLD?

Thank you

With Regards

0 项奖励
回复
1 解答
1,978 次查看
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @mkraj,

You can design a board using LS1028A without CPLD. You can refer to LS1046A FRWY schematic design for implementing the RESET circuitary without using CPLD.

Regards,
Mrudang

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,979 次查看
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @mkraj,

You can design a board using LS1028A without CPLD. You can refer to LS1046A FRWY schematic design for implementing the RESET circuitary without using CPLD.

Regards,
Mrudang

0 项奖励
回复
1,971 次查看
mkraj
Contributor III
Dear Mrudang

Thank you verymuch for your valuable reply.

1. In LS1028A RDB , Few registers are implemented (board control and status register) in CPLD.

If we are removing CPLD, Any major software change is required?

2. Is it ok to go without these BCSR - Board Control / Status Registers in CPLD?

With Regards

Krishnam Raju M
0 项奖励
回复