LS1028A new design without CPLD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1028A new design without CPLD

ソリューションへジャンプ
2,003件の閲覧回数
mkraj
Contributor III

Dear NXP expert

We are planning to go for a new LS1028A based board design without CPLD. We want to implement all reset and control outside CPLD.

Is there any dependency on firmware? Is it mandatory to use CPLD?

Thank you

With Regards

0 件の賞賛
返信
1 解決策
1,970件の閲覧回数
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @mkraj,

You can design a board using LS1028A without CPLD. You can refer to LS1046A FRWY schematic design for implementing the RESET circuitary without using CPLD.

Regards,
Mrudang

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,971件の閲覧回数
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @mkraj,

You can design a board using LS1028A without CPLD. You can refer to LS1046A FRWY schematic design for implementing the RESET circuitary without using CPLD.

Regards,
Mrudang

0 件の賞賛
返信
1,963件の閲覧回数
mkraj
Contributor III
Dear Mrudang

Thank you verymuch for your valuable reply.

1. In LS1028A RDB , Few registers are implemented (board control and status register) in CPLD.

If we are removing CPLD, Any major software change is required?

2. Is it ok to go without these BCSR - Board Control / Status Registers in CPLD?

With Regards

Krishnam Raju M
0 件の賞賛
返信